Technical FAQs

Ask a Question

What is the relationship between Hz and transitions per second for the E5600 digital I/O?

The E5600 pulses are actually transitions.
2 transitions represent 1 Hz.

For example, 5 transitions/sec = 2.5 Hz


Legacy KB System (APS) Data: RESL204434 V1.0, Originally authored by MaTh on 02/01/2011, Last Edited by MaTh on 02/01/2011
Related ranges: E5600
Was this helpful?
What can we do to improve the information ?