Technical FAQs

Ask a Question

Which phase is control power derived from on a PowerLogic E5600?

The two most common E5600 models are Form 9S and Form 36S. Both derive control power from V3. See the diagrams below for wiring schematics (use terminals denoted in red).


Legacy KB System (APS) Data: RESL204334 V1.0, Originally authored by MaTh on 01/19/2011, Last Edited by MaTh on 01/19/2011
Related ranges: E5600
Was this helpful?
What can we do to improve the information ?