Technical FAQs

Ask a Question

What is the maximum Energy value that the E4800 will store/display before rolling over?

The energy register value on the E4800 will reach a maximum at 999,999.999 kWh, once this value is reached the meter will automatically reset (rollover) the registers value to zero and begin accumulating again from there.


Legacy KB System (APS) Data: RESL204329 V1.0, Originally authored by MaTh on 01/18/2011, Last Edited by MaTh on 01/18/2011
Related ranges: EM4800
Was this helpful?
What can we do to improve the information ?