Technical FAQs

Ask a Question

How to generate a recurring report in Advanced Reports which runs monthly and is emailed in Adobe Acrobat format (PDF)

Goals and Symptoms

Summary
This article describes how to create a recurring report in Advanced Reports which is emailed in PDF format.

Causes and Fixes

Resolution

The attached document outlines the procedure to generate a recurring report which is emailed.

For information on enabling SMTP in AR see RESL190871

Attachments

(Removed File URL: 204324_07EE/How_to_generate_a_report_to_run_on_a_monthly_basis_and_email_in_adobe_acrobat_format.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/c649fa39eb576d82c125781c00164559/fl_block_5/0.178?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL204324 V1.0, Originally authored by MaTh on 01/18/2011, Last Edited by MaTh on 01/18/2011
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?