Technical FAQs

Ask a Question

No tables are listed in Display>Tables in System Manager Software(SMS)

Goals and Symptoms

Symptoms
In System Manager Software (SMS) Setup Utility, no tables are listed when going to Display->Tables.

Causes and Fixes

Cause

The user on the server must be a Power User or Administrator in order to view these tables. Alternately, the user account needs access to the PowerLogic\SMS\Tables folder.


Resolution

Grant user access to the PowerLogic\SMS\Tables folder

1) Navigate to PowerLogic\SMS\Tables\ and right-click the Tables folder, select Properties
2) Go to the Security tab
3) Click Add, and find the user on the PC
4) After adding the user, give the user Read, Write, and Modify permission on the folder
5) Click Advanced, check the box next to "Replace permission entries on all child objects with entries shown here that apply to child objects"
6) Click Apply


Legacy KB System (APS) Data: RESL204323 V1.0, Originally authored by MaTh on 01/18/2011, Last Edited by MaTh on 01/18/2011
Related ranges: System Manager 4.3, System Manager 4.2, System Manager 4.0, System Manager 3.3
Was this helpful?
What can we do to improve the information ?