Technical FAQs

Ask a Question

Do PowerLogic meters support the DCF-77 time synchronization signal format?

The following PowerLogic meters support Time Synchronization via the DCF-77 signal format

 
PowerLogic Power Meter PM800 series (with firmware v10.820 or above)
PowerLogic Circuit Monitor CM4000 series
PowerLogic Circuit Monitor CM3000 series

Legacy KB System (APS) Data: RESL204289 V1.0, Originally authored by MaTh on 01/12/2011, Last Edited by MaTh on 01/12/2011
Related ranges: CM4000 series, CM3000 series, PM800 series
Was this helpful?
What can we do to improve the information ?