Technical FAQs

Ask a Question

Error “No connection could be made because the target machine actively refused it 127.0.0.1” in the diagnostics log in Sequnce of Events Recorder (SER) 7.3

Goals and Symptoms

Summary
After a new install of SER 7.3 the PLOPCLogger service is not started. Going to the setup tab at the top of the page, then going to the services link at the bottom left will display an error stating that the service must be started and the error:

No connection could be made because the target machine actively refused it 127.0.0.1

Causes and Fixes

Resolution

To start the PLOPCLogger manually, open Administrative Tools->Services, scroll to the PLOPCLogger service, select and click start. Restarting the computer will also cause the service to come up on boot.


Note:
Rebooting the computer after install, or starting the service manually before going to the setup->services page will avoid this error all together.


Legacy KB System (APS) Data: RESL204025 V1.0, Originally authored by MaTh on 12/02/2010, Last Edited by MaTh on 12/02/2010
Related ranges: Sequence of Events Recorder (SER)
Was this helpful?
What can we do to improve the information ?