Technical FAQs

Ask a Question

CyberSciences SER-3200 is showing an incorrect date when connected to an Arbiter and receiving a good <1ms signal

Goals and Symptoms

Summary
The CyberScience SER-3200 device can receive an IRIG-B time signal from an external Arbiter GPS time source device. The SER-3200 requires an IRIG-B signal which includes both date and time information. Without the Arbiter device configured to include IEEE-1344 extensions, the SER-3200 will show a time quality of Good while having a good time but invalid date.

Causes and Fixes

Cause

The Arbiter time source device does not have IEEE-1344 extensions enabled.


Resolution

Enable the IEEE-1344 time extensions on the Arbiter time source device.


Procedure

Use the Arbiter time source device menu to verify IEEE-1344 extensions have been enabled.

Note:
For more information about the SER-3200 and IEEE-1344 extensions visit the CyberSciences website http://www.cyber-sciences.com/support/technical_irig-b.html


Legacy KB System (APS) Data: RESL204024 V1.0, Originally authored by MaTh on 12/02/2010, Last Edited by MaTh on 12/02/2010
Related ranges: Sequence of Events Recorder (SER)
Was this helpful?
What can we do to improve the information ?