Technical FAQs

Ask a Question

How to determine the Service Pack level of Crystal Enterprise10 (CE10)?

A folder called "Patches" will be created in C:\Program Files\Crystal Decisions\Enterprise 10\Patches. The "Patches" folder will not exists if no service packs have been applied. In this screen capture, Crystal Enterprise 10.0 Service Pack 6 is installed.


Legacy KB System (APS) Data: RESL203939 V1.0, Originally authored by MaTh on 11/19/2010, Last Edited by MaTh on 11/19/2010
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?