Technical FAQs

Ask a Question

What command line parameters are available for the System Manager Software (SMS) Setup Utility shortcut?

The following command line parameters can be applied:
/LOGON username,password
/WORKSPACE "full_file_path"
/DELAY time_delay_in_seconds

*Note: These parameters are case sensitive


Example
C:\POWERLOGIC\SMS\Bin\SMSSetupUtil.exe /LOGON master,master /WORKSPACE "C:\POWERLOGIC\SMS\GFX workspace.wks" /DELAY 30


For more information see "Command Line Parameters" in the SMS Setup Utility Help File.


Legacy KB System (APS) Data: RESL203936 V1.0, Originally authored by MaTh on 11/19/2010, Last Edited by MaTh on 11/19/2010
Related ranges: System Manager 4.3, System Manager 4.2, System Manager 4.0, System Manager 3.3
Was this helpful?
What can we do to improve the information ?