Technical FAQs

Ask a Question

ECMRM/ECM2000 Configuration Tools Download

There are two configuration tools available for programming the ECM modules. One of the tools is the Powerlogic tool (ECM_Config), and the other is directly from the manufacturer of the gateway, Niobrara (PEN_SETUP).
ECM_Config.zipPEN_SETUP.EXE


Legacy KB System (APS) Data: RESL203927 V1.0, Originally authored by MaTh on 11/18/2010, Last Edited by MaTh on 11/18/2010
Related ranges: ECM (ECMRM / ECM2000)
Was this helpful?
What can we do to improve the information ?