Technical FAQs

Ask a Question

When creating/updating a GFX screen, the background needs resizing

Goals and Symptoms

Symptoms
When creating or updating a GFX screen, the background is too small or needs resizing.

or

Some custom GFX objects open up too large/small to be displayed on the screen. The user has to scroll around to see the whole window or zoom out/in.

See screen show below for example.

Causes and Fixes

Cause

A new screen is being added or a existing background is being updated and the size does not match what is needed or what the prior diagram's size is.


Resolution

After opening the GFX screen, press Ctrl-F to allow the user to re-size the background by dragging the corners. Alternatly, go to View-> Fit in Window. The "Zoom Percentage" can be set from the View menu if a fixed percentage is needed instead.


Legacy KB System (APS) Data: RESL203829 V1.0, Originally authored by MaTh on 10/30/2010, Last Edited by MaTh on 10/30/2010
Related ranges: System Manager 4.3, System Manager 4.2, System Manager 4.0, System Manager 3.3
Was this helpful?
What can we do to improve the information ?