Technical FAQs

Ask a Question

"Setup did not locate a suitable domain controller or controller server" error appears when installing Message Queuing in Windows XP

Goals and Symptoms

Symptoms
When installing MSMQ in Windows XP, the following error is displayed:

"Setup did not locate a suitable domain controller or controller server"

Causes and Fixes

Cause

Active Directory Integration is trying to be installed with MSMQ.


Resolution

1. From Windows Control Panel, select Add and Remove Programs
2. Click on Add and Remove Windows Components
3. Select Message Queuing, and click on "Details"



4. Unchecked "Active Directory Integration"


5. Click OK twice, and click Next to continue the installation


Legacy KB System (APS) Data: RESL203721 V1.0, Originally authored by MaTh on 10/16/2010, Last Edited by MaTh on 10/16/2010
Related ranges: System Manager 4.0, System Manager 4.2, System Manager 4.3, SMS Add-on
Was this helpful?
What can we do to improve the information ?