Technical FAQs

Ask a Question

Is it possible to enable "Auto Scrolling" for the EM6400 series display?

Auto Scroll allows the user to monitor a group of Display Pages sequentially, every 5 seconds, without constant key pressing.
There are three different auto scrolling modes:

1. To auto scroll within a specific page group (RMS, THD, INTG, etc..):
Navigate to a particular page in the desired page group, then press the up key continuously for 3 seconds and release. The display will flash AUTO and start to auto scroll within the page group.

2. To auto scroll down the entire column of pages:
Navigate to the desires page, then press the down key continuously for 3 seconds and release. The display will flash AUTO and start to auto scroll through the entire column of pages.

3. To auto scroll through TURBO pages:
Press the TURBO key continuously for 3 seconds and then release.The display will flash AUTO and start to auto scroll through the TURBO pages.

The TURBO pages consist of the following values:
VLL, A, PF
VLN, A, F
VA, W, PF
VA, W,VA
W, VAR, PF
PF1, PF2, PF3
V% 1 2 3
A % 1 2 3
VAd RD TR
MD HR
VAh, Wh
RVAh, RWh
tVAh, tWh

Press any key to revert back to manual scrolling.


Legacy KB System (APS) Data: RESL203615 V1.0, Originally authored by MaTh on 10/01/2010, Last Edited by MaTh on 10/01/2010
Related ranges: EM 6400 DigitAN
Was this helpful?
What can we do to improve the information ?