Technical FAQs

Ask a Question

How to enable and disable EN50160 functionality via System Manager Software (SMS) on a Circuit Monitor 3000/4000 (CM4000/CM3000) or Power Meter 800 (PM800)

Issue
Enabling and Disabling EN50160 functionality via System Manager Software (SMS) 

Product Line
CM3000
CM4000
PM800

Environment
SMS

Cause
Enabling and Disabling EN50160 functionality

Resolution
In the SMS Setup Utility, go to Setup->Device/Routing and double-click on the CM3/CM4/PM8 meter. Under the "Basic Setup" tab click on the "Advanced" button. On the "EN50160" tab check the "Enable EN50160 Evaluation" box to enable EN50160.
EN50160 alarms cannot be enabled under "Onboard Alarms/Events" tab until "enable EN50160" is checked.

EN50160 alarms cannot be disabled under "Onboard Alarms/Events" tab until "enable EN50160" is unchecked.

Was this helpful?
What can we do to improve the information ?