Technical FAQs

Ask a Question

Why does the Active Pager Module (APM) v6.x PowerLogic eSolutions Web banner not stretch across the whole frame?

Example:



This is due to Internet Explorer (IE) 8 incompatibility. To correct this, in IE go to Tools and select Compatibility View or click on the Compatibility View Icon to force IE8 to correctly display the page.



 


Legacy KB System (APS) Data: RESL203483 V1.0, Originally authored by MaTh on 09/21/2010, Last Edited by MaTh on 09/21/2010
Related ranges: SMS Add-on, Paging Module
Was this helpful?
What can we do to improve the information ?