Technical FAQs

Ask a Question

What TCP port does Active Pager Module (APM) 6.x use?

APM 6.0
In Server 2003 and Windows XP, APM uses the TCP port of the default website: 80


APM 6.1, 6.2, & 6.3

In Server 2003 and Server 2008, APM uses TCP port 81
In Windows XP, APM uses the TCP port of the default website: 80


Note: In some manual installations, port 8080 could be used.


Legacy KB System (APS) Data: RESL203482 V1.0, Originally authored by MaTh on 09/21/2010, Last Edited by MaTh on 09/21/2010
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?