Technical FAQs

Ask a Question

Do the ANSI C12.20 and C12.16 standards comply with ANSI C12.1?

The ANSI C12.20 and C12.16 standards do comply with ANSI C12.1.
ANSI C12.16 is no longer used and was combined into ANSI C12.1
ANSI C12.20 is a higher accuracy version of ANSI C12.1

Below is a brief explanation of the standards:
C12.1 Code for Electricity Metering (covers all types of meters/instruments)
C12.16 Solid-State Electricity Meters (rolled into C12.1, only dealt with solid-state meters)
C12.20 For electricity Meters -- 0.2 and 0.5 Accuracy Classes (C12.1 plus higher accuracy requirements)

Document Change History

Date and Initials Comments
2010-10-29 DRM * Changed range association away from "Metering application \ Metering device selection" in preparation for the removal of this range and the product family under which it is classified.

Legacy KB System (APS) Data: RESL203478 V2.0, Originally authored by MaTh on 09/21/2010, Last Edited by DaMi on 11/03/2010
Related ranges: Standards Applied to Power Management PRODUCTS
Was this helpful?
What can we do to improve the information ?