Technical FAQs

Ask a Question

What type of OPC Server is used by SMS OPC Server/Matrikon OPC server?

SMS OPC Server uses OPC DA (OPC Data Access), whereas Active Pager Module (APM) uses OPC AE (OPC Alarm Event).


Legacy KB System (APS) Data: RESL203477 V1.0, Originally authored by MaTh on 09/21/2010, Last Edited by MaTh on 09/21/2010
Related ranges: Paging Module, SMS Add-on
Was this helpful?
What can we do to improve the information ?