Technical FAQs

Ask a Question

Unable to define a rate for a custom quantity when generating a Energy Cost Summary Report in Advanced Reports

Goals and Symptoms

Symptoms
When generating a Energy Cost Summary Report in Advanced Reports (AR) for a device in which custom quantities have been added in System Manager Software (SMS), AR will not allow a rate to be associated to the custom quantity.

The EDIT field is not present on the Define Charges page of the report wizard. Consequently, there is no charge of any value associated with the quantity. When pressing on the Next button, the following error is returned:

"Length cannot be less than zero. Parameter name: length"

The report cannot be completed.

Causes and Fixes

Cause

The Energy Cost Summary report only allows rates to be defined for quantities that are created with the Information Type of "Cumulative Consumption".

This issue is most commonly encountered when custom quantities are defined in SMS for third party devices that have been added into the system. By default, when adding a new custom quantity, the Information Type is set to "Unassigned". The Information Type must be set to "Cumulative Consumption" which corresponds to energy, a cumulative quantity.


Resolution

Modify the Information Type field

1. Open SMS Setup Utility
2. Go to Setup > Custom Quantities...
3. Highlight the specific custom quantity in question
4. Change the Information Type field in the drop down window to "Cumulative Consumption"
5. Press the Update button and then close the Setup Custom Quantities window
6. The PowerLogic Network Server Service (PLNS) must be restarted for these changes to take affect


Example Screen Shots

Custom Quantity Configuration for "Custom_Qty_1" is incorrect and generates the error:



Custom Quantity Configuration for "Custom_Qty_2" is correct:



The proper Define Charges window for the Energy Cost Summary report:


 


Legacy KB System (APS) Data: RESL203375 V1.0, Originally authored by MaTh on 09/08/2010, Last Edited by MaTh on 09/08/2010
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?