Technical FAQs

Ask a Question

Active Pager Module (APM) 6.x millisecond patch for alarm timestamps

This patch displays the APM alarm timestamp at the millisecond level for those alarms in SMS that are in millisecond format.
This patch is only intended for APM v 6.0, 6.1, and 6.2.

Example:
Default Format - 8/10/2010 11:46 AM
Format After Patch - 8/10/2010 11:46:22.110 AM

To deploy the patch:

1. Stop APM and OPC Logger services.
2. Rename the PLOpc.Common.dll in the [install location]\SMS OPC AE Server\ folder and in the [install location]\Active Pager Module\ folder.
3. Copy the included dll in the [install location]\SMS OPC AE Server\ folder and also in the [install location]\Active Pager Module\ folder.
4. Start the APM and OPC Logger services.

APM Millisecond Fix.zip


Legacy KB System (APS) Data: RESL203166 V1.0, Originally authored by MaTh on 08/25/2010, Last Edited by MaTh on 08/25/2010
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?