Technical FAQs

Ask a Question

Digital input status changes are not reflected in Sequence of Events Recorder (SER) 7

Goals and Symptoms

Symptoms
When the status of a CM3/CM4 digital input changes, the change is not shown in SER. In addition, no errors are present in SER.

Causes and Fixes

Cause

The Circuit Monitor's input is incorrectly configured


Resolution

Set the CM's digital input Mode to SER
Enable the CM's onboard SER Data Log with a non-zero record count.


Legacy KB System (APS) Data: RESL203164 V1.0, Originally authored by MaTh on 08/25/2010, Last Edited by MaTh on 08/25/2010
Related ranges: Sequence of Events Recorder (SER)
Was this helpful?
What can we do to improve the information ?