Technical FAQs

Ask a Question

Com Surrogate error when browsing System Manager Software Webclient (SMSWeb)

Goals and Symptoms

Symptoms
When browsing to the System Manager Software (SMS) Web Client (SMSWeb), the user receives the following error:

Com Surrogate Error
Faulting application dllhost.exe, version 5.1.2600.5512, faulting module wam.dll, version 5.1.2600.5512, fault address 0x000074af.

Causes and Fixes

Cause

Is most circumstances, this is caused by a non-patched version of Windows.


Resolution

Run the Microsoft Windows Update utility to obtain all the latest Microsoft patches.


Legacy KB System (APS) Data: RESL203158 V1.0, Originally authored by MaTh on 08/24/2010, Last Edited by MaTh on 08/24/2010
Related ranges: System Manager 4.3, System Manager 4.2, System Manager 4.0
Was this helpful?
What can we do to improve the information ?