Technical FAQs

Ask a Question

"Could not create object named "Scripting.FileSystemObject" Windows Script Host error when repairing Crystal Enterprise 10 (CE10)

Goals and Symptoms

Symptoms
When running the Crystal Enterprise 10 Repair, Windows Script Host generates the following error message:

Could not create object named "Scripting.FileSystemObject

Causes and Fixes

Cause

Windows Scripting Host is disabled


Resolution

Download and install Windows Script Host version 5.7 (WSHv5.7)

Windows XP version
Windows Server 2003 version


Legacy KB System (APS) Data: RESL203154 V1.0, Originally authored by MaTh on 08/21/2010, Last Edited by MaTh on 08/21/2010
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?