Technical FAQs

Ask a Question

What Mounting Brackets should be used with the Energy Meter, Enercept Meter, or 3090SCCT series current transformers (CTs)?

Issue:
A customer may want to know the part numbers for mounting brackets for current transformers

Product Line:
Energy Meter Current Transformers
Enercept Meter Current Transformers
3090SCCT-  Current Transformers

Environment:
Metering and Power Monitoring

Cause:
Current transformers are often hung on the conductors they are to monitor, but there may be the need to secure them within electrical enclosures for the sake of safety, identifiability, order, and clean installation.

Resolution:
The 3050EMBK1 (for 1 CT), 3050EMBK2 (for 2 CTs), or 3050EMBK3 (for 3 CTs) can be used with any CT from the Energy meter, Enercept meter, or 3090SCCT series that is above 100A.

This is because the base of the CT is same for the Medium and Large style CT.

Was this helpful?
What can we do to improve the information ?