Technical FAQs

Ask a Question

Unable to set probes to Phase C in the PowerLogic E4800 Configuration Utility

Goals and Symptoms

Symptoms
In the PowerLogic E4800 Configuration Tool, Phase C is not an option under the Meter Points (Circuits) tab.

Causes and Fixes

Resolution

This has been correct in version 1.3 of the E4800 Configuration Tool. Click here to download v1.3.


Legacy KB System (APS) Data: RESL203092 V1.0, Originally authored by MaTh on 08/12/2010, Last Edited by MaTh on 08/12/2010
Related ranges: E4800
Was this helpful?
What can we do to improve the information ?