Technical FAQs

Ask a Question

Conzerv EM6400 Instruction Bulletin for firmware 03.02.xx

This documentation is for use with Conzerv EM6400 meters of firmware 03.02.xx. It is NOT for use with firmware 03.03.xx and above.
EM 6400 Manual (Firmware 03.02.xx).pdf


Legacy KB System (APS) Data: RESL203086 V1.0, Originally authored by MaTh on 08/11/2010, Last Edited by MaTh on 08/11/2010
Related ranges: EM 6400 DigitAN
Was this helpful?
What can we do to improve the information ?