Technical FAQs

Ask a Question

PowerLogic EM4800 Configuration Tool v1.40 Build 1060 (Windows 7 Compatible) download

Latest version as of 09/27/2010
Attached is the EM4800 Configuration Tool. Uninstall any prior version before installing v1.4.
The EM4800 tool is usable with both the EM4800 and E4800 meters.

Note: Regarding the use of the Meter Configuration tool in Windows 7, Version 1.20 Build 1046 of the EM4800 Configuration Tool which is shipped with the meter does not support Windows 7 Operating System. The attached version of the EM4800 Configuration Tool, Version 1.40 Build 1060 supports both .Net Framework v3.5 and the Windows 7 Operating System.

EM4800Config.zipEM4800Config.zip


Legacy KB System (APS) Data: RESL203083 V3.0, Originally authored by MaTh on 08/11/2010, Last Edited by MaTh on 05/02/2013
Related ranges: EM4800
Was this helpful?
What can we do to improve the information ?