Technical FAQs

Ask a Question

How to change the Branch Current Monitor (BCM) or Branch Circuit Power Meter (BCPM) circuit orientation (Top Feed, Bottom Feed, Sequential, or Odd/Even)

Branch Current Monitor (BCM) Orientation
The circuit orientation is determined by dip switch settings on the BCM board. Refer to the BCM Circuit Orientation.pdf document for dip switch settings.

BCM Circuit Orientation.pdf


Note: Changing the circuit orientation is only available on BCMs with a firmware revision of 1.10 or greater. The firmware revision number is stored in holding registers 50 and 51. For example if register 50 = 1 and register 51 = 9, the firmware revision is 1.9.


Branch Circuit Power Meter (BCPM) Orientation

The circuit orientation is determined by the value held in register 6.

0 = Top Feed (Default)
1 = Bottom Feed
2 = Sequential
3 = Single Row: Odd/Even

Refer to the BCPM Circuit Orientation.pdf document for register settings.

BCPM Circuit Orientation.pdf


Legacy KB System (APS) Data: RESL202916 V1.0, Originally authored by MaTh on 07/14/2010, Last Edited by MaTh on 07/14/2010
Related ranges: BCPM(Branch Circuit Power Meter), BCM (Branch Current Monitor)
Was this helpful?
What can we do to improve the information ?