Technical FAQs

Ask a Question

What are the different E4800 meter configuration models?

The E4800 has 5 different "modes" of operation specified by the Model #. Here is a breakdown of what the different modes are used for:


1P-12 - This configuration is used for measuring 2-pole breakers in a single-phase panel.
1P-24 - This configuration is used for measuring 1-pole breakers in a single-phase panel.
2P-12 - This configuration is used for measuring 2-pole breakers in a three-phase panel.
2P-24 - This configuration is used for measuring 1-pole breakers in a three-phase panel.
3P-08 - This configuration is used for measuring 3-pole breakers in a three-phase panel.


Legacy KB System (APS) Data: RESL202907 V1.0, Originally authored by MaTh on 07/13/2010, Last Edited by MaTh on 07/13/2010
Related ranges: E4800
Was this helpful?
What can we do to improve the information ?