Technical FAQs

Ask a Question

Trend data in ION EEM v3.9 and above does not show up or is improperly offset.

This can be caused by the timezone being set improperly for the source in the ION EEM Admin Tool. To resolve this problem, login to the ION EEM Admin Tool and go to the Source Node Hierarchies plugin. Click on the sources tab and check that timezone is set properly for the devices experiencing the issue.
________________________________________
Date Created: June 3, 2010
Last Revised: June 4, 2010
Public
Original Author: MN
All content © 1992-2010 Schneider Electric


Legacy KB System (APS) Data: RESL202440 V1.0, Originally authored by LaAd on 06/05/2010, Last Edited by LaAd on 06/05/2010
Related ranges: EEM V3.9
Was this helpful?
What can we do to improve the information ?