Technical FAQs

Ask a Question

"The page cannot be found" error message when accessing the System Manager Software (SMS) webclient

When accessing the SMS webclient (web client), the user receives the following error message:
The page cannot be found


This error is seen most commonly when Active Server Pages is prohibited in Internet Information Services in Windows 2003.


Resolution

In Internet Information Services, click on Web Service Extensions and allow "Active Server Pages"


Legacy KB System (APS) Data: RESL202130 V1.0, Originally authored by MaTh on 04/29/2010, Last Edited by MaTh on 04/29/2010
Related ranges: System Manager 4.0, System Manager 4.2, System Manager 4.3
Was this helpful?
What can we do to improve the information ?