Technical FAQs

Ask a Question

Why is the "Run this report automatically on a scheduled basis" checkbox greyed out in Information Manager?

There are two reason why a user would be unable to schedule reports in Information Manager.
1. The user is connected to the SMS server via a remote desktop or terminal server connection. Windows does not allow creation of scheduled tasks via these connections methods.

2. The user is logged in directly at the machine, but improper Windows login credentials have been supplied to Information Manager. To correct this, open Information Manager, go to File->Change Windows Account Info and supply a valid Windows Administrator login and password.


Legacy KB System (APS) Data: RESL202107 V1.0, Originally authored by MaTh on 04/24/2010, Last Edited by MaTh on 04/24/2010
Related ranges: System Manager 4.3, System Manager 4.2, System Manager 4.0, System Manager 3.3
Was this helpful?
What can we do to improve the information ?