Technical FAQs

Ask a Question

Can ECC or EGX communication gateways read Powerlogic device registers in the webpage?

The EGX100, EGX300, and PM8ECC all have a built-in Modbus/Powerlogic register read interfaces. The ECC21 and EGX400 do not have a register read interface, but by using the Web Page Generator, predefined web pages can be created which will read device information from downstream devices. The EGX200 does not offer the ability to read device register information.


Legacy KB System (APS) Data: RESL201833 V1.0, Originally authored by MaTh on 03/30/2010, Last Edited by MaTh on 03/30/2010
Related ranges: EGX400, PM8ECC, EGX300, EGX200, EGX100, ECC21
Was this helpful?
What can we do to improve the information ?