Technical FAQs

Ask a Question

What edition of SQL Server 2000 is installed with System Manager Software (SMS) Professional Edition (PE) 4.0?

The SQL Server 2000 edition is operating system dependant:
Windows XP Professional installs SQL2K_Personal edition
Windows 2000/2003 Server installs SQL2K_Standard edition


Legacy KB System (APS) Data: RESL201502 V1.0, Originally authored by MaTh on 03/02/2010, Last Edited by MaTh on 03/02/2010
Related ranges: System Manager 4.0
Was this helpful?
What can we do to improve the information ?