Technical FAQs

Ask a Question

How to change the Schneider Electric company logo on Tenant Metering Software (TMS) 1.5 bills.

The Schneider Electric company logo can be changed to reflect the tenant billing company.
The logo is located at: C:\PowerLogic\TenantMetering\LOGO.jpg

The customer can modify this file or swap out thier own logo in this one's place.

Image Requirements

File name must be named LOGO.jpg
Image size* must be: Width = 211, Height = 50

*Any other image size will be expanded/condensed to 211x50 pixels.


Legacy KB System (APS) Data: RESL201466 V1.0, Originally authored by MaTh on 02/26/2010, Last Edited by MaTh on 02/26/2010
Related ranges: Tenant Metering Software
Was this helpful?
What can we do to improve the information ?