Technical FAQs

Ask a Question

Does having a main breaker instead of lugs or a 200% rated neutral affect the ULc or CSA rating of a NQ or NF panel with a BCM42 or BCPM?

The BCM42/BCPM is a ULc and CSA listed component. As long as no modifications have been made to the product, it can be installed into a ULc or CSA assembly without affecting the ratings. Having a breaker rather than lugs or having a 200% neutral will not change this.


Legacy KB System (APS) Data: RESL201058 V1.0, Originally authored by MaTh on 01/19/2010, Last Edited by MaTh on 01/19/2010
Related ranges: BCPM(Branch Circuit Power Meter), BCM (Branch Current Monitor)
Was this helpful?
What can we do to improve the information ?