Technical FAQs

Ask a Question

How to get ION Enterprise Vista to show timestamps in 24 hour (military time) format.

This can be accomplished by changing the server time to the 24 hour time format. To do this change the regional and language time settings to reflect the time properly.
1) Open the Windows Control Panel
2) Go to Regional and Language Options
3) On the Regional Options tab choose customize
4) Go to the time tab and change the time format


Date Created: January 11, 2010
Last Revised: January 12, 2010
Public
Original Author: MN
All content © 1992-2010 Schneider Electric


Legacy KB System (APS) Data: RESL201019 V1.0, Originally authored by MiNe on 01/12/2010, Last Edited by MiNe on 01/12/2010
Related ranges: ION Enterprise V6.0, ION Enterprise V5.6, ION Enterprise V5.5
Was this helpful?
What can we do to improve the information ?