Technical FAQs

Ask a Question

What are the default user privilege levels in PowerLogic SCADA?

Issue
What are the default user privilege levels in PowerLogic SCADA.

Product Line
Powerlogic SCADA 7.x
PowerScada Expert 8.x

Environment
User creation. 

Cause
User wishes to create new users using the default user privileges. 

Resolution
There are 5 different default user privileges in PowerLogic SCADA as per below.
Note: The privilege levels need to be manually entered. They are not part of the project by default in most cases. 
 

Access Right
User Levels / Global Privileges
Description
Operator1
Operator2
Engineer
Administrator
Kernel
 
2
4
6
7
8
Circuit Breaker, Switch control
 
X
X
X
X
Alarms acknowledgment
X
X
X
X
X
Alarm configuration
 
 
X
X
X
Add/remove log-in users
 
 
 
X
X
Shutdown Runtime    
X
X
X

Was this helpful?
What can we do to improve the information ?