Technical FAQs

Ask a Question

Can I use DM6000 and PM1000 Series for single phase applications?

Yes, provided you select 1 Phase for 1-Phase 2-Wire system in the program menu - Setup


Legacy KB System (APS) Data: RESL200920 V1.0, Originally authored by DaMi on 01/07/2010, Last Edited by DaMi on 01/07/2010
Related ranges: DM6000 series, PM1000 series
Was this helpful?
What can we do to improve the information ?