Technical FAQs

Ask a Question

Script error during a report pack installation to ION Enterprise Web Reporter


=================================
Internet Explorer Script Error
-----------------------------------------
An error has occurred in the script on this page.
Line: 313
Char: 5
Error: Object doesn't support this property or method
Code: 0
URL: http://localhost/Web/Modules/Reports/Upload/UploadReportPack.aspx?rx=6512169551621&ReportType=ReportServerReport

Do you want to continue running scripts on this page?

<Yes> <No>
=================================

If you have a script error as above during your report pack installation please follow the next procedure.

 

1. Go to your Internet Explorer 7 Tools Pop-up Blocker Pop-up Blocker Settings.

 

2. Add your server name, localhost, 127.0.0.1 as per below.

 


2. Add your server name, localhost, 127.0.0.1 as per below.

Or you can simply disable the Pop-up Blocker option as per below.

Document Change History

Date and Initials Comments
2010-Jan-29 DRM * Updated document according to recommendation by YJ. Suggested resolution was improved by using a more sophisticated and robust method than the original version suggested.

Last Revised: 2010-Jan-29 by DRM based on input from YJ

Original Author: YJ

Public

All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL200780 V3.0, Originally authored by KBAdPM on 12/23/2009, Last Edited by DaMi on 01/30/2010
Related ranges: ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?