Technical FAQs

Ask a Question

"There was an error retrieving data from the server: Automation server can't create object." error message when accessing the View/Schedule tab in Advanced Reports (AR)

Goals and Symptoms

Symptoms
When accessing the View/Schedule tab in Advanced Reports, the user receives the following error message:

There was an error retrieving data from the server: Automation server can't create object.

The Create, Edit, and Admin tabs are all accessible

Facts and Changes

PRODUCTS Affected
SMS 4.0, 4.2, and 4.3 with Advanced Reports

Causes and Fixes

Cause

The EnterpriseFramework.dll and WebReporting.dll's registration is corrupted.


Resolution

Re-register the Crystal EnterpriseFramework.dll and WebReporting.dll

1. Close all open Internet Explorer sessions of Advanced Reports
2. Go to the Windows Start Menu and choose 'Run...'
3. Type the following and click 'Ok':

REGSVR32 "C:\Program Files\Crystal Decisions\Enterprise 10\win32_x86\EnterpriseFramework.dll"

4. Go to the Windows Start Menu and choose 'Run..'
5. Type the following and click 'Ok':

REGSVR32 "C:\Program Files\Common Files\Crystal Decisions\2.5\bin\WebReporting.dll"

6. Restart Internet Information Services (IISRESET from the Windows command prompt) and re-launch Advanced Reports


Legacy KB System (APS) Data: RESL200634 V2.0, Originally authored by MaTh on 12/01/2009, Last Edited by MaTh on 01/21/2011
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?