Technical FAQs

Ask a Question

Will ION EEM v3.95 work with Windows Server 2008 64-bit operating system (OS)?

ION EEM v3.95 is not officially supported on Windows Server 2008 64-bit OS. ION EEM 3.95 SP1 is supported on Windows Server 2008 32-bit OS.

Date Created: November 25, 2009
Last Revised: November 25, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL200593 V1.0, Originally authored by MiNe on 11/26/2009, Last Edited by MiNe on 11/26/2009
Related ranges: EEM V3.95
Was this helpful?
What can we do to improve the information ?