Technical FAQs

Ask a Question

Can the ECC21 display ITIC / CBEMA curves?

Goals and Symptoms

Goal
To add the ITIC / CBEMA webpage option to the ECC21.

Causes and Fixes

Cause

By default the ECC21 card does not have the CBEMA curve webpage pre-loaded


Resolution

FTP the ITIC.htm file to the ECC21 to enable ITIC / CEBEMA graphs

1. Download the attached ITIC.htm file to the root of C:\
2. Open a Windows Command Prompt (cmd)
3. Enter "ftp xxx.xxx.xxx.xxx" where the x's correspond to the IP address of the ECC21
4. When prompted, enter the ECC user name "admin"
5. When prompted, enter the admin password. The default password is "admin"
6. Enter "send C:\itic.htm"


ITIC.htm



Example ITIC graph


Legacy KB System (APS) Data: RESL200365 V1.0, Originally authored by MaTh on 10/28/2009, Last Edited by MaTh on 10/28/2009
Related ranges: ECC21
Was this helpful?
What can we do to improve the information ?