Technical FAQs

Ask a Question

Tenant Metering Software (TMS) 1.x left menu bar is partially blocked from view

Goals and Symptoms

Symptoms
The Tenant Metering Software (TMS) 1.x left menu bar is partially blocked from view. See the following screen capture for comparison:


 

Causes and Fixes

Cause

The computers DPI display settings are set to a nonstandard value


Resolution

Change the computer's DPI settings to 96 DPI:

1. Open Windows Control Panel from the Start menu
2. Double-click on 'Display Settings'
3. In the 'Settings' tab, click the 'Advanced' button
4. Change the 'DPI setting' to "Normal size (96 DPI)"

TMS 1.x is designed to only run in 96 DPI mode.


Legacy KB System (APS) Data: RESL200323 V1.0, Originally authored by MaTh on 10/23/2009, Last Edited by MaTh on 10/23/2009
Related ranges: Tenant Metering Software
Was this helpful?
What can we do to improve the information ?