Technical FAQs

Ask a Question

"Destination DLL disabled" error in Advanced Reports (AR) when scheduling a report

Goals and Symptoms

Symptoms
When scheduling a report and choosing a destination in Advanced Reports, the report fails with one of the following error messages:

destination DLL disabled. CrystalEnterprise.Smtp:
destination DLL disabled. CrystalEnterprise.Ftp:
destination DLL disabled. CrystalEnterprise.Smtp:

Causes and Fixes

Cause

The Crystal Report Job Server's SMTP, FTP, or Unmanaged Disk destinations are disabled. Note: These destinations are disabled by default.


Resolution

Enable the Crystal Report Job Server's destinations

1. In Advanced Reports, click on the 'Admin' tab
2. From the Crystal Enterprise Admin Launchpad, click 'Crystal Management Console' (CMC)
2. Log in to the CMC using an Administrator account
3. Click on 'Servers'
4. Click 'servername.reportjobserver'
5. Click the 'Destinations' tab
6. Place a checkmark in each box under 'Selected' and click on 'Enable'
7. By clicking on DiskUnmanaged, FTP, or SMTP, default settings such as folder location, FTP Host, and SMTP server can be configured


Legacy KB System (APS) Data: RESL200272 V1.0, Originally authored by MaTh on 10/17/2009, Last Edited by MaTh on 10/17/2009
Related ranges: System Manager 4.0, System Manager 4.3, System Manager 4.2
Was this helpful?
What can we do to improve the information ?