Technical FAQs

Ask a Question

Does PowerLogic SCADA support waveform data of ION meters?

No, Powerlogic SCADA (PLS) currently does not support the waveform data from ION meters; valid through PLS v7.10 SR3.
Waveforms from the following devices are currently supported as of v7.10 SR3: Circuit Monitor 3000s, Circuit Monitor 4000s, Power Meter 800s, and Sepam 20s, 40s, and 80s.


Legacy KB System (APS) Data: RESL200266 V2.0, Originally authored by KBAdPM on 10/16/2009, Last Edited by MaTh on 12/01/2010
Related ranges: PowerLogic SCADA 7.1
Was this helpful?
What can we do to improve the information ?