Technical FAQs

Ask a Question

What is the maximum number of characters allowed for the computer name when installing System Manager Software (SMS)?

The Maximum number of characters allowed for the computer name when installing System Manager Software (SMS) is 15. This is a Microsoft Windows limitation.


Legacy KB System (APS) Data: RESL200104 V1.0, Originally authored by MaTh on 09/25/2009, Last Edited by MaTh on 09/25/2009
Related ranges: System Manager 3.3, System Manager 4.0, System Manager 4.2, System Manager 4.3
Was this helpful?
What can we do to improve the information ?