Technical FAQs

Ask a Question

Tenant Metering Software (TMS) 1.x: "PowerLogic.TenantMetering.Comms.MeterCommsApp.exe - Fatal Error: CLR error: 80004005"

Goals and Symptoms

Symptoms
User sees the following error message when starting the PowerLogic.TenantMetering.Comms.MeterCommsApp.exe. This executable starts automatically when the user logs onto the computer.




The Windows Application Event Log shows the following information about the error:

Facts and Changes

PRODUCTS Affected:
TMS 1.0 TMS 1.5

Causes and Fixes

Cause

The PowerLogic.TenantMetering.Comms.MeterCommsApp.exe has been set to run in 'Windows Compatibility Mode'.


Resolution

Modify the properties of the PowerLogic.TenantMetering.Comms.MeterCommsApp.exe to not use Compatibility Mode

1. Right-click on the file C:\POWERLOGIC\TenantMetering\bin\PowerLogic.TenantMetering.Comms.MeterCommsApp.exe and choose Properties
2. Click on Compatibility tab
3. Un-check all options
4. Click OK
5. Double-click on the PowerLogic.TenantMetering.Comms.MeterCommsApp.exe to re-start the program



Legacy KB System (APS) Data: RESL200083 V1.0, Originally authored by MaTh on 09/24/2009, Last Edited by MaTh on 09/24/2009
Related ranges: Tenant Metering Software
Was this helpful?
What can we do to improve the information ?