Technical FAQs

Ask a Question

Is a tax rate entered as a decimal or percentage in Tenant Metering Software (TMS) 1.5?

ANOTHER COMMON QUESTION AROUND THIS SAME ISSUE: Why is the tax charge so high in the Tenant Metering Software (TMS) v1.0.1 bill?

 


ANSWER: A tax rate must be entered as a decimal, not a percentage. For example, a tax rate of 6% would be entered as '0.06', not '6'.

PRODUCTS Affected:
TMS 1.0 TMS 1.5

Legacy KB System (APS) Data: RESL200069 V2.0, Originally authored by MaTh on 09/23/2009, Last Edited by DaMi on 10/15/2009
Related ranges: Tenant Metering Software
Was this helpful?
What can we do to improve the information ?